Win10 IoT Use Cases for Cloud connectivity Using MQTT on iMX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Win10 IoT Use Cases for Cloud connectivity Using MQTT on iMX

1,705 次查看
purnankg
NXP Employee
NXP Employee

Are there any reference applications/use cases already available that uses MQTT protocol and connect to some of the cloud service providers like Azure/AWS/Google. #Win10IoT #iMX

标签 (1)
0 项奖励
回复
2 回复数

1,535 次查看
amisaify
Contributor I

Hello, can provide more information on which specific Azure Services you are interested in using with your Windows application on the IoT Device?

Microsoft Azure Documentation | Microsoft Docs 

Azure IoT Hub that enables an operator to connect, monitor and control IoT devices at scale. It supports MQTT.

Azure IoT Hub Documentation - Tutorials, API Reference | Microsoft Docs 

0 项奖励
回复

1,535 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Purnank G,

There is a Windows 10 IoT Core BSP here: https://github.com/ms-iot/imx-iotcore

However, it does not have support to connect to cloud services right of the box. I would recommend contacting Microsoft as they may provide more insight on these capabilities.

Regards,

0 项奖励
回复