Win10 IoT Use Cases for Cloud connectivity Using MQTT on iMX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Win10 IoT Use Cases for Cloud connectivity Using MQTT on iMX

1,687 Views
purnankg
NXP Employee
NXP Employee

Are there any reference applications/use cases already available that uses MQTT protocol and connect to some of the cloud service providers like Azure/AWS/Google. #Win10IoT #iMX

Labels (1)
0 Kudos
Reply
2 Replies

1,517 Views
amisaify
Contributor I

Hello, can provide more information on which specific Azure Services you are interested in using with your Windows application on the IoT Device?

Microsoft Azure Documentation | Microsoft Docs 

Azure IoT Hub that enables an operator to connect, monitor and control IoT devices at scale. It supports MQTT.

Azure IoT Hub Documentation - Tutorials, API Reference | Microsoft Docs 

0 Kudos
Reply

1,517 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Purnank G,

There is a Windows 10 IoT Core BSP here: https://github.com/ms-iot/imx-iotcore

However, it does not have support to connect to cloud services right of the box. I would recommend contacting Microsoft as they may provide more insight on these capabilities.

Regards,

0 Kudos
Reply