Will imx287 support the capactive touchscreen?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will imx287 support the capactive touchscreen?

ソリューションへジャンプ
1,520件の閲覧回数
ask
Contributor III

Will imx287 support the capactive touchscreen?

I read imx287 will not support the capactive touch screen. Is it right?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,402件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

i.MX28 supports resistive touch screens natively through built-in ADC.

For capacitive touch support, external touch controller connected via I2C or SPI is required.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,403件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

i.MX28 supports resistive touch screens natively through built-in ADC.

For capacitive touch support, external touch controller connected via I2C or SPI is required.

0 件の賞賛
返信