Wifi connect issue !

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wifi connect issue !

2,816 次查看
liyu1
Contributor III

Hi all !


     I found a problem, wiif connection issue .  When I connect to WiFi hotspots, reported a warning !


   

<4>RTL871X: assoc success

<4>------------[ cut here ]------------

<4>WARNING: at net/wireless/sme.c:482 __cfg80211_connect_result+0x2f4/0x32c()

<4>Modules linked in: 8188eu

<4>[<c0054044>] (unwind_backtrace+0x0/0x138) from [<c008c1b8>] (warn_slowpath_common+0x4c/0x64)

<4>[<c008c1b8>] (warn_slowpath_common+0x4c/0x64) from [<c008c1ec>] (warn_slowpath_null+0x1c/0x24)

<4>UpdateHalRAMask8188EUsb => mac_id:0, networkType:0x0b, mask:0x000fffff

<4>     ==> rssi_level:0, rate_bitmap:0x000ff015

<4>[<c008c1ec>] (warn_slowpath_null+0x1c/0x24) from [<c069e3a0>] (__cfg80211_connect_result+0x2f4/0x32c)

<4>[<c069e3a0>] (__cfg80211_connect_result+0x2f4/0x32c) from [<c06893f4>] (cfg80211_process_rdev_events+0x1e0/0x204)

<4>[<c06893f4>] (cfg80211_process_rdev_events+0x1e0/0x204) from [<c0686ec0>] (cfg80211_event_work+0x24/0x54)

<4>[<c0686ec0>] (cfg80211_event_work+0x24/0x54) from [<c00a66f0>] (process_one_work+0x12c/0x494)

<4>[<c00a66f0>] (process_one_work+0x12c/0x494) from [<c00a6bc8>] (worker_thread+0x170/0x3cc)

<4>[<c00a6bc8>] (worker_thread+0x170/0x3cc) from [<c00aacbc>] (kthread+0x80/0x88)

<4>[<c00aacbc>] (kthread+0x80/0x88) from [<c004d408>] (kernel_thread_exit+0x0/0x8)

<4>---[ end trace 14efbc2d6eba2439 ]---



     

标签 (2)
0 项奖励
回复
4 回复数

2,273 次查看
haoranwang
NXP Employee
NXP Employee

Hi,

    Could you please share us more information about your platform? Such as the board, chip, wifi model and Android Release version.

    Thanks!

0 项奖励
回复

2,273 次查看
liyu1
Contributor III

hardware : imx6q

os :android 4.4.2

wifi module :rtl8188etv

0 项奖励
回复

2,273 次查看
haoranwang
NXP Employee
NXP Employee

Hi Liyu,

     I think the driver you use is not from the Realtek official one.

     Please use the official drivers instead of the open source one.

     Thanks

0 项奖励
回复

2,273 次查看
wilsonchen
Contributor III

HI,LI:

     I want to know the way how to solve the problem  in android 4.4.2 wifi softap mode! .  I also use the rtl8188eu module。  thanks!

The above problem ,you can check the imx6_android_defconfig:

CONFIG_CFG80211=y

CONFIG_MAC80211=y


We can exchange ideas about this .



0 项奖励
回复