WiFi chipset supporting AP mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

WiFi chipset supporting AP mode

1,043 次查看
jaffinmk
Contributor III

Hello all

I am in search of a Wifi chipset which can be interfaced with iMX6 QuadPlus Sabre board easily (I am running linux 3.14) and which supports dual band frequency and AP mode and has a good performance. I have found BCM4330 chipset. Is there any other better option. Also is there any USB adapter with BCM4330 to connect with the board and test it out before buying the chipset. Any information regarding this will be helpful.

标签 (2)
0 项奖励
回复
1 回复

810 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jaffin

L3.14.xx early versions supported Atheros AR6003 please refer to attached

Linux Manual Chapter 48 AR6003 WiFi.

http://www.nxp.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&Parent_nodeId=13376994810717061... 

for broadcom wifi options one can check

https://wikidevi.com/wiki/Broadcom#USB 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复