WiFi SDIO interface on uSDHC2 i.MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WiFi SDIO interface on uSDHC2 i.MX6Q

1,853 Views
atillametetured
Contributor V

Hello,

Is there anything that prevents connecting the SDIO interface of the WiFi chip to the i.MX6 over the uSDHC2?

Is there a dedicated interrupt pin for this purpose?

Kind Regards,

Mete

Labels (2)
0 Kudos
Reply
1 Reply

1,572 Views
art
NXP Employee
NXP Employee

Q. Is there anything that prevents connecting the SDIO interface of the WiFi chip to the i.MX6 over the uSDHC2?

A. No.

Q. Is there a dedicated interrupt pin for this purpose?

A. No.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply