About ASI master clock of MX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About ASI master clock of MX6UL

ソリューションへジャンプ
1,265件の閲覧回数
yuuki
Senior Contributor II

Dear all,

I want to use SAI of i.MX6UL.

I refer to Chapter 43 of RM.
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf
- Chapter 43 Synchronous Audio Interface (SAI)

I have some questions.

<Q1>
I understand the Master Clock of SAI is generated by SAIx_CLK_ROOT.
Is SAIx_CLK_ROOT connected directly with Master Clock of SAIx?

<Q2>
In MCLK Select field of I2Sx_TCR2 register, audio Master Clock option can be chosen.
However, I cannot find the explanation about these options.

Would you tell me the point where this is explained?

<Q3>
In MCLK Select of the I2Sx_RCR2 register, would you tell me the concrete clock name of "00:Bus Clock selected"?

May I have advice?

Best Regards,
Yuuki

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
968件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Yuuki

If you refer to section 18.3 “CCM Clock Tree” of the same Reference Manual you will see the origins and destinations of each clock signal, including SAI1_CLK_ROOT, SAI2_CLK_ROOT and SAI3_CLK_ROOT.

Then, on section 18.4, the Table 18-3 shows the CCM output clocks' system-level connectivity. The following picture shows the SAI’s clocks:

SAI clocks.png


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
968件の閲覧回数
570035964
Contributor I

Hi:

Why the SAI1_MCLK Can't output to the Pin.

my configuration:

Use Pad : CSI_DATA01,  Mode(ALT6), PAD_CTL (Pull up with 47kohm, SPEED_3_max_200MHz, Fast_Slew_rate)

The other signal of the SAI (include BCLK、SYNC、DATA) are all output correctly.

Help me out,Tks

0 件の賞賛
返信
968件の閲覧回数
kenmeng
Contributor II

HI

are you solved this problem?

i have same issue. if you solved,please share it with everyone!

0 件の賞賛
返信
969件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Yuuki

If you refer to section 18.3 “CCM Clock Tree” of the same Reference Manual you will see the origins and destinations of each clock signal, including SAI1_CLK_ROOT, SAI2_CLK_ROOT and SAI3_CLK_ROOT.

Then, on section 18.4, the Table 18-3 shows the CCM output clocks' system-level connectivity. The following picture shows the SAI’s clocks:

SAI clocks.png


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
968件の閲覧回数
yuuki
Senior Contributor II

Dear CarlosCasillas-san,

Thank you for your support.

I understood that those clock were connected like the following figure.

ASI Mclk.png

- MCLK of each ASI is supplied from ASIx_CLK_ROOT.
- Clock source (SAIx_CLK_ROOT) is chosen by MSEL field.
- The Bus clock means AHB CLK(AHB_CLK_ROOT).

Is my understanding right?

Best Regards,

Yuuki

0 件の賞賛
返信
968件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Yuuki,

Yes, you are right!


Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信