Wi-Fi Display Sink in i.MX6 Android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wi-Fi Display Sink in i.MX6 Android

1,378件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi.
i have seen Wi-Fi Display Sink in i.MX6 Android article on below link.
https://community.nxp.com/docs/DOC-102180

I want do to on my board. I have imx6sabresd board with android 4.4.3. How to do wifi display on this??

Any package i need to add in the android source.?

How to do the board as receiver display.?

0 件の賞賛
返信
2 返答(返信)

758件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi aravinthkumar

Wi-Fi Display Sink Feature Package is KK extended feature package.

This package is available to approved customers (send request

to L2manager-android@freescale.com).

Note, starting with Android M6.0.1_2.0.0 the extended feature package

is rolled into the main Android BSP release.

Android M6.0.1_2.0.0 GA Release Announcement

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

758件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi igorpadykov​,

Thanks for your quick response.

How to make the board as receiver display.?

Regards,

Aravinth

0 件の賞賛
返信