Why use about Debug LED and SDXC Power Control Inverter? - I.MX6DL(Automotive)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why use about Debug LED and SDXC Power Control Inverter? - I.MX6DL(Automotive)

Jump to solution
4,308 Views
inhojeon
Contributor III

Hi all,

I wondering about 'Debug LED and SDXC Power Control Inverter'  of I.MX6DL(Automotive) SABRE Bd Circuit.

And I wondering about what purpose of 'SDa_RST_B'  and 'SDa_PWROFF' , 'USER_LED', 'P3V3_SDa_SWITCHED'

And, Is 'Debug LED and SDXC Power Control Inverter' circuit must to use?

Best Regards,

Inho Jeon. 

Labels (1)
1 Solution
4,113 Views
Yuri
NXP Employee
NXP Employee

Hello,

  If Your design is not intended to use both voltages 3.3V and 1.8 V for SD 
interface and SD supply will not be switched on / off  - the mentioned solution
with switched supply may be ommited.  In such case You may use P3V3_DELAYED
instead of P3V3_SDa_SWITCHED.

Regards,

Yuri.

View solution in original post

7 Replies
4,113 Views
inhojeon
Contributor III

Hi, Yuri!

I have a question about "SDa (SD3) power source for MX6 I/O. Required for SDXC USH-1 I/O logic level change " of i.MX6DL(Automotive) that refer to SABRE BD Schematics( 6 of 22 pages).

I want to NVCC_SD3 is P1V8GEN4 for SDXC(high speed SD IO level 1.8V).

So, I'll designed just R613 & R640 for NVCC_SD3 level control by add & del R640,R631 without U508(ADG849) and SDa_VSELECT(SD3_VSEL_GPIO_18),  Is it right way?

Plaese, Infome me that questions, ASPA.

Best Regards,

Inho Jeon.

0 Kudos
Reply
4,113 Views
Yuri
NXP Employee
NXP Employee

Hello,

  To get P1V8GEN4 for SDXC : populate R631, assuming R640 is removed, U508 is not needed. 

Have a great day,
Yuri

4,113 Views
inhojeon
Contributor III

Hi, Yuri!

Thank you for your reply.

You mean just need to parts of R640 & R631 for driving SD or SDXC memory cards, no need to  parts of 'U508' ,'R633', 'C625',R638 and net of 'SDa_VSELECT(SD3_VSEL_GPIO_18)', is that right?

Best regards,

Inho Jeon

0 Kudos
Reply
4,113 Views
Yuri
NXP Employee
NXP Employee

Yes, just direct connection for corresponding power rail.

~yuri.

4,113 Views
Yuri
NXP Employee
NXP Employee

Hello,

1.
Dedug LED is separate scheme, that – generally has no any concern to SDXC support.

2.

  For the SDXC card support it is required to apply 1.8V supply voltage.

GPIO_18 (ALT2: VSELECT of usdhc3) is used to control the NVCC_SD3 for 3.3V and 1.8V voltage select.
SD3_RST(inverted to SDa_PWROFF) is used to control / switch the SD Card Power (P3V3_SDa_SWITCHED).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,113 Views
inhojeon
Contributor III

Hi Yuri,

Thank you for your reply.

You mean if not use SDXC it is not necessary, is that right?

And, if not use SDXC, how to design about  "SDa_RST_B(SD3_RST)" , "P3V3_SDa_SWITCHED" ?

Best Regards,

Inho Jeon

0 Kudos
Reply
4,114 Views
Yuri
NXP Employee
NXP Employee

Hello,

  If Your design is not intended to use both voltages 3.3V and 1.8 V for SD 
interface and SD supply will not be switched on / off  - the mentioned solution
with switched supply may be ommited.  In such case You may use P3V3_DELAYED
instead of P3V3_SDa_SWITCHED.

Regards,

Yuri.