Hello Everybody
I tried to find best kernel.I have three different kernel version which i tested on same board IMX6Q with QT cinematic experience app.There are huge differences each others. Firstly Kernel 3-14-28 version better than others because yellow ball is moving fluently and smooth.And This kernel can reach 60 FPS. But Secondly Kernel 4-1-15 the ball is freze sometimes like blink when it is moving at 52 FPS.Strangely The ball is moving faster than others.Finally Kernel 4-14-69 have same problem like 4-1-15 but 4-14-69 can reach just 30 fps .
I expected new version kernels would be better.
What is the problem?
I need to solve freze and increase FPS?
How can i solve them?
Kernel Versions | 3-14-28 | 4-1-15 | 4-14-69 |
Video | Fluent | Freeze | Freeze |
FPS | 60 | 52 | 30 |
Ball Speed | Normal | Faster | Normal |
Kernel Version 3-14-28
Kernel Version 4-1-15
Kernel Version 4-14-69
Hi Muhammet
reason may be that new kernels include many bug fixes, which are described
in Release Notes included in linux documentation, for example check Table 9. New features
"Bug Fixes" attached Release Notes
i.MX Software and Development Tools | NXP
also one can check https://community.nxp.com/message/1031643?commentID=1031643#comment-1031643
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Muhammet
for tq-github software suggest to apply to tq-support.
NXP supports only linux from source.codeaurora.org/external/imx/linux-imx
repository linux-imx - i.MX Linux kernel
i.MX Software and Development Tools | NXP
Best regards
igor