Why native build depend required in Apache2 build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why native build depend required in Apache2 build

1,383 Views
dougbailey
Contributor III

I am trying to build an Apache 2.2 image and I am looking at the Apache 2.4 recipe as a basis. I see that Apache 2.4 depends on the native build of apache. can someone explain why the native build is required for the cross-compile build?

Labels (2)
0 Kudos
Reply
1 Reply

969 Views
b36401
NXP Employee
NXP Employee

Perhaps it uses native Apache installation to build configuration of cross-compiled Apache.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply