Why native build depend required in Apache2 build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why native build depend required in Apache2 build

1,326件の閲覧回数
dougbailey
Contributor III

I am trying to build an Apache 2.2 image and I am looking at the Apache 2.4 recipe as a basis. I see that Apache 2.4 depends on the native build of apache. can someone explain why the native build is required for the cross-compile build?

ラベル(2)
0 件の賞賛
返信
1 返信

912件の閲覧回数
b36401
NXP Employee
NXP Employee

Perhaps it uses native Apache installation to build configuration of cross-compiled Apache.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信