Why ioctl asrc convert call is loading the main thread?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why ioctl asrc convert call is loading the main thread?

3,772 Views
phanikumar
Contributor III

Hi all,

I am using hardware asrc on imx6 ul free scale board by using linux ioctl driver calls. There are two threads in my application in which one is main thread and other one is asrc thread. In the asrc thread, I am calling ioctl asrc convert driver function. In general, once I have data I will call ioctl function, otherwise the asrc thread will go into conditional wait. The code inside the ioctl function is supposed to be light weight so that the main thread can carry other tasks while hardware asrc is converting the data. But, I see there is a serious loading happens and my main thread is running slowly. When the ioctl call in the asrc thread is switched off, the main thread runs at a faster rate which is what needed even in the presence of ioctl call. Could anyone please help to understand this behavior of ioctl call...Thanks

Labels (4)
7 Replies

3,401 Views
yifangguo-b4310
NXP Employee
NXP Employee

Hi,

   Actually,  there is a unit test about ASRC driver in your target  image root fs, the path is "/unit_tests/mxc_asrc_test.out" , you can run it :

$ . /unit_tests/autorun-asrc.sh

And test this for check the driver if available.  Otherwise, it is your thread issue.

3,401 Views
phanikumar
Contributor III

Hi Yifang Guo,

Thanks for your suggestions... The asrc after testing independently is working fine. There is no issue with quality. My goal is to use it as a parallel resource. So, I am calling it from a separate thread. I suppose the function ioctl for asrc convert should not take much cycles from the core after it is called.  Because I want to use the core for other tasks running in parallel through threading. Please correct me if there is any mistake..Thanks..

0 Kudos
Reply

3,401 Views
yifangguo-b4310
NXP Employee
NXP Employee

Hi ,

   ASRC driver implement CONVERT by hardware module (Asynchronous Sample Rate Converter), it don't spend ARM core  executing cycles when   convert  sample rate.   You can  use ARM core  to deal with other task simultaneously.

You test  call  ioctl  ASRC_CONVERT periodically in your thread. e.g:

while(1){

ioctl(fd_asrc, ASRC_CONVERT, &buf_info);

msleep(100);   //  escape time from this thread; then CPU can call other threads.

}

Attatched "mxc_asrc_test" source code for reference.

0 Kudos
Reply

3,400 Views
phanikumar
Contributor III

Hi Yifang,

Which header file has this function msleep(). Is this compulsory to keep?

0 Kudos
Reply

3,400 Views
yifangguo-b4310
NXP Employee
NXP Employee

  #include <unistd.h>

google linux msleep function.

msleep(100);  can  escape time from this thread; then CPU can call other threads

0 Kudos
Reply

3,400 Views
phanikumar
Contributor III

Hi jimmychan,

Thanks for your reply..

The ioctl call goes as follows ..

err = ioctl(fd_asrc, ASRC_CONVERT, &buf_info);

fd_asrc is the id of the hardware asrc

ASRC_CONVERT is the command

struct asrc_convert_buffer buf_info has the details of input and output addresses with the lengths as well

This call is used in mxc_asrc driver code.. I would be looking forward for your views and suggestions.. thanks..

0 Kudos
Reply

3,400 Views
jimmychan
NXP TechSupport
NXP TechSupport

could you tell me more details? which driver are you talking about? which ioctl function you called that had serious loading?