Hi, below log show that u-boot spl execute two times. can you give me some advice? scu fw version is v1.1, source code build.
U-Boot SPL 2018.03-g1c71305-dirty (May 08 2019 - 11:51:01 +0000)
Trying to boot from MMC1
Load image from MMC/SD 0x46000
U-Boot 2018.03-g1c71305-dirty (May 08 2019 - 11:51:01 +0000)
CPU: Freescale i.MX8QXP revB A35 at 1200 MHz at 40C
Model: Freescale i.MX8QXP MEK
Board: iMX8QXP MEK
Boot: MMC0
DRAM: 3 GiB
U-Boot SPL 2018.03-g1c71305-dirty (May 08 2019 - 11:51:01 +0000)
Trying to boot from MMC1
Load image from MMC/SD 0x46000
U-Boot 2018.03-g1c71305-dirty (May 08 2019 - 11:51:01 +0000)
CPU: Freescale i.MX8QXP revB A35 at 1200 MHz at 40C
Model: Freescale i.MX8QXP MEK
Board: iMX8QXP MEK
Boot: MMC0
DRAM: 3 GiB
WIFI_EN = 0
MMC: SDHC_0 set clock parent failed!(error = 10)
SDHC_1 set clock parent failed!(error = 10)
FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
Failed (-5)
TX PLL is not locked.
In: serial@5a060000
Out: serial@5a060000
Err: serial@5a060000
BuildInfo:
- SCFW 65afe5f6, SECO-FW 31fabbff, IMX-MKIMAGE 34b84aaa, ATF 84a79ee
- U-Boot 2018.03-g1c71305-dirty
flash target is MMC:0
Net: [board_eth_init] 284
FEC1 MXC: board_eth_init:failed
Board Net Initialization Failed
No ethernet found.
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
=>