Hi All,
I am using kernel verson 3.14.28 with dts support. When i am doing cat /sys/class/gpio/gpio157
root@imx6_fs_wcam:/home# cat /sys/class/gpio/gpio157/value
0 (when low)
root@imx6_fs_wcam:/home# cat /sys/class/gpio/gpio157/value
536870912 (when high)
Why instead of 1 we are getting 536870912 this value here?
If any one knows can you explain me.
Thanks
Lavanya
解決済! 解決策の投稿を見る。
This issue has already been fixed in recent kernel versions. Please try 4.1 kernel instead.
This issue has already been fixed in recent kernel versions. Please try 4.1 kernel instead.
Here is the upstream commit that fixes this issue:
commit 25b35da7f4cce82271859f1b6eabd9f3bd41a2bb
Author: Linus Walleij <linus.walleij@linaro.org>
Date: Wed Feb 5 14:08:02 2014 +0100
gpio: generic: clamp retured value to [0,1]
The generic GPIO would return 0 for low generic GPIO, and
something != 0 for high GPIO. Let's make this sane by clamping
the returned value to [0,1].
Reported-by: Evgeny Boger <boger@contactless.ru>
Reviewed-by: Alexandre Courbot <acourbot@nvidia.com>
Signed-off-by: Linus Walleij <linus.walleij@linaro.org>
diff --git a/drivers/gpio/gpio-generic.c b/drivers/gpio/gpio-generic.c
index 8c778af..d815dd2 100644
--- a/drivers/gpio/gpio-generic.c
+++ b/drivers/gpio/gpio-generic.c
@@ -139,7 +139,7 @@ static int bgpio_get(struct gpio_chip *gc, unsigned int gpio)
{
struct bgpio_chip *bgc = to_bgpio_chip(gc);
- return bgc->read_reg(bgc->reg_dat) & bgc->pin2mask(bgc, gpio);
+ return !!(bgc->read_reg(bgc->reg_dat) & bgc->pin2mask(bgc, gpio));
}
static void bgpio_set(struct gpio_chip *gc, unsigned int gpio, int val)
Hi Fabio Estevam,
Thankyou, i will follow this
Linux document can give you explaination
Documentation/gpio/sysfs.txt
allow userspace to reconfigure this GPIO's direction.
"value" ... reads as either 0 (low) or 1 (high). If the GPIO is configured as an output, this value may be written;
any nonzero value is treated as high.
If the pin can be configured as interrupt-generating interrupt
and if it has been configured to generate interrupts (see the description of "edge"), you can poll(2) on that file and
poll(2) will return whenever the interrupt was triggered. If
you use poll(2), set the events POLLPRI and POLLERR. If you
use select(2), set the file descriptor in exceptfds. After
poll(2) returns, either lseek(2) to the beginning of the sysfs
file and read the new value or close the file and re-open it
to read the value.
"edge" ... reads as either "none", "rising", "falling", or