Why does add IC add IC NC7WV16 between IMX8 mini Enthernet ENET_RX[0:3] and AR8031

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why does add IC add IC NC7WV16 between IMX8 mini Enthernet ENET_RX[0:3] and AR8031

1,414 次查看
wangchqin
Contributor I

Why does add IC add IC NC7WV16 between IMX8 mini Enthernet ENET_RX[0:3] and AR8031  , if I want  change AR8031 to  RTL 8211E  ,  if the  IC NC7WV16 is need ?

0 项奖励
回复
3 回复数

1,409 次查看
joanxie
NXP TechSupport
NXP TechSupport

refer to the schematic,

Drivers are included in the receive path due to long signal paths
and board-to-board connector. Adopters should place the PHY and
processor on the same board, and eliminate the drivers. Refer to
Atheros documentation for additional guidance

 

0 项奖励
回复

1,406 次查看
wangchqin
Contributor I

if I use another PHY  as RTL8211F (with normal  driver) ,  and let  the MAC and PHY  in one board without B to B connector ,  can I  omit   IC NC7WV16 ?

0 项奖励
回复

1,399 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes you can omit it

 

0 项奖励
回复