Why do you parse data-lanes property in device tree as u32 instead of as an array?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why do you parse data-lanes property in device tree as u32 instead of as an array?

1,496件の閲覧回数
AnthonyZ
Contributor III

driver source: imx8-mipi-csi2-sam.c
kernel version: imx 5.4.70_2.3.0
The data-lanes property is parsed as u32 in imx8-mipi-csi2-sam.c. This very unusual in comparison to many other documented drivers including other imx drivers using this property.
The driver in imx8-media-dev.c e.g. also calls a function "v4l2_fwnode_endpoint_parse" which parses the same property (data-lanes) in a different way.
This does not lead to any error as v4l2 just initializes falsely interpreted data, but it is still not according to the v4l2-framework and may cause unwanted side-effects in the future.

Hence, the question is: Is there any reason for interpreting data-lanes as u32 instead of as an u32_array?

Regards,
Anthony

0 件の賞賛
返信
1 返信

1,485件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

You can see this kernel  wiki https://www.kernel.org/doc/html/v4.18/media/kapi/v4l2-fwnode.html 

The u32_array size is decided by num_data_lanes.

The u32  data-lanes in dts  just numbers of datalanes.

The node of data-lanes is parsed into num_lanes

of_property_read_u32(node, "data-lanes", &state->num_lanes);

So there is no problem

 

BR

Zhiming

0 件の賞賛
返信