Why clk_enable and clk_disable can't be called in interrupt context for freescale Linux BSP -blog archive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why clk_enable and clk_disable can't be called in interrupt context for freescale Linux BSP -blog archive

2,169件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

    In Freescale Linux BSP code, clk_enable() in clock.c (in folder /kernel_imx/arch/arm/plat-mxc) is not allowed to be used in ISR context as attached real code below.

 if (in_interrupt()) {
  printk(KERN_ERR " clk_enable cannot be called in an interrupt context\n");
  dump_stack();
  BUG();
 }

 

    The main reason behind doing this is to allow for voltage scaling as part of clk_enable()/clk_disable() functions. Voltage scaling uses the Regulator APIs which cannot be called in an ISR context.
For example, in clk_enable/clk_disable, set_low_bus_freq() and set_high_bus_freq() have chance to be called, and in these functions, regulator_set_voltage() sometimes will be called.

    For a temp solution, If you wants to call clk_enable/clk_disable in UART ISR context, I think you can define two new functions, just remove the bus_freq related codes. (Because the UART clock is not DVFS or bus freq related, and other BSP driver will continue to use the original clk apis, there will be no impact)

 

int clk_enable2(struct clk *clk)
{
 unsigned long flags;
 int ret = 0;

 if (clk == NULL || IS_ERR(clk))
  return -EINVAL;

 spin_lock_irqsave(&clockfw_lock, flags);

 ret = __clk_enable(clk);

 spin_unlock_irqrestore(&clockfw_lock, flags);

 return ret;
}
EXPORT_SYMBOL(clk_enable2);

 

void clk_disable2(struct clk *clk)
{
 unsigned long flags;

 if (clk == NULL || IS_ERR(clk))
  return;

 spin_lock_irqsave(&clockfw_lock, flags);

 __clk_disable(clk);

 spin_unlock_irqrestore(&clockfw_lock, flags);
}

EXPORT_SYMBOL(clk_disable2);

タグ(1)
0 件の賞賛
返信
0 返答(返信)