Which serial interface is suitable for my protocol (i.MX8 ULP)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which serial interface is suitable for my protocol (i.MX8 ULP)?

645 次查看
paullegart
Contributor II

My processor is i.MX8 ULP.

I've got a chip which has a master SSI interface like that:

 

SSI_diagram.png

There are 3 lines in the interface: clock (CLK), serial data (DATA) and FrameSync (FS). Each frame contains three words of 16 bits each. FS is active on the last bit of the frame. Data is streaming (no gaps).

So which interface should I use to reiceive data from this chip? It actually doesn't matter which core should manage the signal but A35 is preferrable.

As I guess I2S is not suitable because it can manage 2 channels only. Regarding SPI interface I have no idea how to set it up for streaming (no gaps) mode.

标记 (1)
0 项奖励
回复
2 回复数

624 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I think it should be almost the same situation with SAI or SPI interfaces since you need to create a new driver to support that device in your design.

Which IC do you want to interface? Maybe there is something that could be used as reference in our side.

Best regards.

0 项奖励
回复

591 次查看
paullegart
Contributor II

The chip is AD9874. The topic is just more about hardware support of this interface rather the driver but I would glad to hear any suggestions about everything.

0 项奖励
回复