Which parameter to cross compile?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which parameter to cross compile?

1,059 Views
paolosantini
Contributor III

I work on a SBC Variscite based on IMX6UL; to replace the second splashscreen I have to compile a .C file using "configure" command.

Some indications about how to cross compile from Linux ? My environment is:

/opt/fslc-x11/2.2.1/environment-setup-armv7at2hf-neon-fslc-linux-gnueabi

Some one could help me?

Labels (2)
0 Kudos
Reply
1 Reply

958 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Paolo Santini,

There is a Hello World example on the following training:

https://community.nxp.com/docs/DOC-95225

There is also an example on this thread’s comments, which is a bit more up to date.

https://community.nxp.com/thread/394804

I hope this helps!

Regards,

0 Kudos
Reply