Which kernel to use for imx6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which kernel to use for imx6?

4,683 次查看
randysilagi
Contributor II

Hello,

I am kinda lost with all the kernel available for iMX6 ...

I don't find any note saying what is the kernel to use for iMX6...

I know this has been asked before however, I did not find a suitable answer.  Maybe if I ask is in different way..

There is so many git repository ...

->git://git.freescale.com/imx/linux-2.6-imx.git (so many branch on it ...)

->git://git.freescale.com/auto/linux.git (so many branch on it ...)

->git://github.com/Freescale/linux-mainline.git (so many branch on it ...)

So, I have downloaded:

->buildroot.git - Automotive Buildroot Tree​    2015.08-rc1_s32v234_0.6

Should I use the Linux from the auto git tree?  git.freescale.com/git/cgit.cgi/auto/linux.git/

or from the Imx git? git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/

How do I tell which is the most recent stable version?  Does _ga mean stable release?  Same question applies to u-boot.  Use the one in the auto get or the imx one?  I am building for an i.mx6sx Sabre SD.

Thanks for your help.

Randy Silagi

标签 (2)
0 项奖励
回复
2 回复数

1,495 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Randy

please follow Yocto guide provided in BSP documentation

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

or look at

linux-2.6-imx.git - Freescale i.MX Linux Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,495 次查看
nelson_lin
Contributor I

Hi igor,

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0) is not available. May it be redirect to the link below?

0 项奖励
回复