Hi Hyun-mo
>Which feature do I have to enable to use the LVDS0 of LCD without the IT6263
>in /vendor/nxp-opensource/kernel_imx?
I am afraid it is not supported, so it is necessary to make software changes.
One can start with linux imx8qm-mek-jdi-wuxga-lvds1-panel.dtsi
https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek-j...
it uses panel-simple.c driver, custom lcd timings can be adjusted in " struct display_timing jdi_tx26d202vm0bwa_timing" :
https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/panel/panel-simple.c?h=imx...
In general, in Android Automotive default image, M4 will be responsible for displaying
at the starting stage. Therefore a lot of resources is assigned to M4 first, and the dts for
Automotive is a little different.
Best regards
igor