Which Linux-5.10 branch in the linux-imx repo is recommended to run on i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which Linux-5.10 branch in the linux-imx repo is recommended to run on i.MX6

1,044件の閲覧回数
MikeQi
Contributor I

Hi,

We plan to port Linux-5.10 onto our hardware platform which is based on i.MX6.

There are only two Linux-5.10 branches in the https://source.codeaurora.org/external/imx/linux-imx repo, their names are git.kernel.org/linux-stable/linux-5.10.y and lf-5.10.y. 

Which branch is recommended to run on i.MX6?  Do I need to wait for a Linux-5.10 branch whose name looks like imx_5.10.xx_x.x.x? I find some Linux-5.4 branches named in that way, e.g. imx_5.4.70_2.3.0 in the repo.

Thanks in advance

ラベル(2)
0 件の賞賛
返信
0 返答(返信)