IMX6ULL BB RevC Ethernet not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL BB RevC Ethernet not working

441 Views
arnoutdiels
Contributor III

Hi,

Just mentioning that I just ordered an IMX6ULL, and running the stock SD card or even the latest linux kernel, fails to bring up the ethernet ports.

From other posts I was able to deduce that the following patch was required to fix the phy on the revC of the breakout board:

http://git.freescale.com/git/cgit.cgi/imx/meta-fsl-bsp-release.git/plain/imx/meta-bsp/recipes-kernel... 

Hope this helps someone, and why is this only present as a shady BSP patch and not inside of the imx kernel?

Kind regards,

Arnout

0 Kudos
1 Reply

299 Views
art
NXP Employee
NXP Employee

This fix for the new silicon revision of the KSZ8081 PHY was just implemented and is not included into the BSP yet. Hope it will be done in the nearest future.


Have a great day,
Artur

0 Kudos