Whether GPIO_3 CKO2 can give SYS_MCLK for SGTL5000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Whether GPIO_3 CKO2 can give SYS_MCLK for SGTL5000

882件の閲覧回数
v_hariharan_ex1
Contributor I

Hi,

Interface details,

GPIO_3 CKO2 is connected with SYS_MCLK of SGTL5000. We tried to generate MCLK from IMX6, but we could not able get any clock on CLKO2 pin.

&ssi2 {     
        assigned-clocks = <&clks IMX6QDL_CLK_PLL4>,
                          <&clks IMX6QDL_PLL4_BYPASS>,
                          <&clks IMX6QDL_CLK_SSI2_SEL>,
                          <&clks IMX6QDL_CLK_CKO2_SEL>,
                          <&clks IMX6QDL_CLK_CKO2>;
        assigned-clock-parents = <&clks IMX6QDL_CLK_OSC>,
                                 <&clks IMX6QDL_CLK_PLL4>,
                                 <&clks IMX6QDL_CLK_PLL4_AUDIO_DIV>,
                                 <&clks IMX6QDL_CLK_CKO2_SEL>;
        assigned-clock-rates = <737280000>, <0>, <0>;
        status = "okay";
};

Configured PIN MUX,

MX6QDL_PAD_GPIO_3__CCM_CLKO2            0x130b0

        codec: sgtl5000@2a {
                compatible = "fsl,sgtl5000";
                reg = <0x2a>;
                clocks = <&clks IMX6QDL_CLK_CKO2>
        };

Please share your inputs how to configure the CLK Output on GPIO_3 for SYS_MCLK of SGTL5000.

Thanks,

Hariharan.V.

ラベル(3)
0 件の賞賛
返信
1 返信

783件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hariharan

necessary configurations can be made in uboot board file (in folder uboot/boards/freescale/board_name/)

as not always such configuration is supported through dts file. Uboot Porting Guide can be found in

Linux documentation on
i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信