Where the MAC Address is stored in Nitrogen 6Lite boards?.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where the MAC Address is stored in Nitrogen 6Lite boards?.

Jump to solution
1,671 Views
andresgonzalez
Contributor II

Hi.r

We are creating an Ethernet Driver for the Nitrogen 6Lite boards which uses a i.MX6 Solo processor and we want to obtain the MAC address that was assigned by the vendor to the board.

However we don't know where the MAC address is stored. When we read PAUR and PALR we always get 0x00 in all bytes, so we are supposing the MAC address is assigned in other place.

Thanks for your help.

Tags (2)
1 Solution
1,469 Views
EricNelson
Senior Contributor II

That's exactly right. The mac address is stored in OTP fuses reserved for this purpose (Bank 4, registers 2 and 3 in U-Boot addressing).

View solution in original post

0 Kudos
Reply
4 Replies
1,469 Views
sinanakman
Senior Contributor III

Hi Andres

This is from their blog : http://boundarydevices.com/fuse-command/

Does that help ?

Regards

Sinan Akman

1,469 Views
andresgonzalez
Contributor II

Thanks for your help, this is very helpful.

0 Kudos
Reply
1,470 Views
EricNelson
Senior Contributor II

That's exactly right. The mac address is stored in OTP fuses reserved for this purpose (Bank 4, registers 2 and 3 in U-Boot addressing).

0 Kudos
Reply
1,469 Views
andresgonzalez
Contributor II

Thanks.

0 Kudos
Reply