Where is u-boot.imx generated in yocto build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is u-boot.imx generated in yocto build

1,912 Views
knightstreet
Contributor I

Hi,

 

I am attempting to generate the .imx images (u-boot and kernel) suitable for use with the uuu tool. The board is based in the imx6ulevk.

I bitbake the yocto setup using this:

MACHINE=imx6ulevk DISTRO=fsl-imx bitbake core-image-minimal

I want to flash to NAND so I have set the following variables up:

UBOOT_CONFIG = "nand"
UBOOT_CONFIG[nand] = "mx6ul_14x14_evk_config,nand"

This generates the u-boot-nand-2020.04-r0.bin file which is great and the relevant wic file but I also need the .imx version to use with UUU or it complains about the IVT header.

I understand that mkimage needs to be invoked but I don't know the configuration option within the image/board config to create these files. Could anybody explain the process needed to generate these files?

My endgame is to invoke uuu using the following command -

uuu -b nand u-boot.imx core-image-minimal-imx6ulevk.wic.gz

Please let me know also if this is the right uuu command set for flashing to nand.

Thank you

 

Labels (3)
0 Kudos
Reply
1 Reply

1,885 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello knightstreet,

You have to be sure that the board is booting form NAND before using the uuu is involve many configuration since uboot and you have to manipulate the UUU software to complete this task.

 

Regards

 

0 Kudos
Reply