Where is ddr related code in codebase?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where is ddr related code in codebase?

1,523 次查看
tony_l_cai
Contributor III

Hi, All

     I want to know,on Freescale platform, the path about DDR related code in its codebase, have some specific c files for DDR such as initialization? If have ,plz give me some path,3Q!

标签 (2)
标记 (3)
0 项奖励
回复
3 回复数

1,453 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tony

ddr initialization is performed in file

uboot/board/freescale/mx6q_sabresd/flash_header.S

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,453 次查看
tony_l_cai
Contributor III

Hi, igor

I want to know the position about ddr driver, could you give me some info?

3Q~

Best Wishes,

Tony

发件人: igorpadykov

发送时间: 2015年1月6日 16:08

收件人: Tony L Cai

主题: Re: - Where is ddr related code in codebase?

<https://community.freescale.com/>

Where is ddr related code in codebase?

reply from igorpadykov<https://community.freescale.com/people/igorpadykov?et=watches.email.thread> in i.MX Community - View the full discussion<https://community.freescale.com/message/467089?et=watches.email.thread#467089>

0 项奖励
回复

1,453 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tony

there is no "ddr driver".

Best regards

igor

0 项奖励
回复