Where can I download the Android JB4.2.2 source?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I download the Android JB4.2.2 source?

2,659件の閲覧回数
zjuhasz
Contributor I

Hi,

Does anyone knows where the JB4.2.2 source is? The link 'IMX6_JB422_100_ANDROID_SOURCE' on page https://community.freescale.com/docs/DOC-94798 is not working.

Thanks.

ラベル(1)
0 件の賞賛
返信
12 返答(返信)

1,821件の閲覧回数
Yuri
NXP Employee
NXP Employee

  I will send you the link.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,821件の閲覧回数
sheldonlrucker
Contributor IV

Hello Yuri,

Could you send me the link as well?  I need access to the JB4.2.2 source.  My email is sheldon_rucker@hotmail.com.

Thank you,

Sheldon

0 件の賞賛
返信

1,821件の閲覧回数
Yuri
NXP Employee
NXP Employee

Done !

~Yuri.

0 件の賞賛
返信

1,821件の閲覧回数
liuvincent
Contributor I

Hi Yuri,

I am working with iMX 6 EVB and need Android JB4.2.2 source also.

Can you please send my the link too?

Thank you,

Vincent

0 件の賞賛
返信

1,821件の閲覧回数
Yuri
NXP Employee
NXP Employee

Your e-mail ?

~Yuri.

0 件の賞賛
返信

1,821件の閲覧回数
charliechang
Contributor II

Could you send the android 4.2.2 source code download link to me? charliechang@aplex.com.tw

Thank you.

0 件の賞賛
返信

1,821件の閲覧回数
Yuri
NXP Employee
NXP Employee

Done !

0 件の賞賛
返信

1,821件の閲覧回数
liuvincent
Contributor I

Hi Yuri,

My email address is vincent.liu@u-blox.com

Thank you,

Vincent

0 件の賞賛
返信

1,821件の閲覧回数
saurabh206
Senior Contributor III

Hi

Z

If you want JB4.3 than please follow

https://community.freescale.com/docs/DOC-99115

Thanks

Saurabh

0 件の賞賛
返信

1,821件の閲覧回数
zjuhasz
Contributor I

Thanks Saurabh, but the problem is I need exactly the 4.2.2 version as other components I must use depend on this particular version. I might be able to move up t 4.3 or 4.4 later but first I must build m system using 4.2.2.

0 件の賞賛
返信

1,821件の閲覧回数
saurabh206
Senior Contributor III

Hi,

You can download 4.3, once the download completed you can modified the manifest.xml for 4.2.2.

It should work.

Thanks

Saurabh

1,821件の閲覧回数
zjuhasz
Contributor I

Thanks, I will try that then.

0 件の賞賛
返信