Where can I download the Android JB4.2.2 source?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I download the Android JB4.2.2 source?

2,413 Views
zjuhasz
Contributor I

Hi,

Does anyone knows where the JB4.2.2 source is? The link 'IMX6_JB422_100_ANDROID_SOURCE' on page https://community.freescale.com/docs/DOC-94798 is not working.

Thanks.

Labels (1)
0 Kudos
Reply
12 Replies

1,575 Views
Yuri
NXP Employee
NXP Employee

  I will send you the link.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,575 Views
sheldonlrucker
Contributor IV

Hello Yuri,

Could you send me the link as well?  I need access to the JB4.2.2 source.  My email is sheldon_rucker@hotmail.com.

Thank you,

Sheldon

0 Kudos
Reply

1,575 Views
Yuri
NXP Employee
NXP Employee

Done !

~Yuri.

0 Kudos
Reply

1,575 Views
liuvincent
Contributor I

Hi Yuri,

I am working with iMX 6 EVB and need Android JB4.2.2 source also.

Can you please send my the link too?

Thank you,

Vincent

0 Kudos
Reply

1,575 Views
Yuri
NXP Employee
NXP Employee

Your e-mail ?

~Yuri.

0 Kudos
Reply

1,575 Views
charliechang
Contributor II

Could you send the android 4.2.2 source code download link to me? charliechang@aplex.com.tw

Thank you.

0 Kudos
Reply

1,575 Views
Yuri
NXP Employee
NXP Employee

Done !

0 Kudos
Reply

1,575 Views
liuvincent
Contributor I

Hi Yuri,

My email address is vincent.liu@u-blox.com

Thank you,

Vincent

0 Kudos
Reply

1,575 Views
saurabh206
Senior Contributor III

Hi

Z

If you want JB4.3 than please follow

https://community.freescale.com/docs/DOC-99115

Thanks

Saurabh

0 Kudos
Reply

1,575 Views
zjuhasz
Contributor I

Thanks Saurabh, but the problem is I need exactly the 4.2.2 version as other components I must use depend on this particular version. I might be able to move up t 4.3 or 4.4 later but first I must build m system using 4.2.2.

0 Kudos
Reply

1,575 Views
saurabh206
Senior Contributor III

Hi,

You can download 4.3, once the download completed you can modified the manifest.xml for 4.2.2.

It should work.

Thanks

Saurabh

1,575 Views
zjuhasz
Contributor I

Thanks, I will try that then.

0 Kudos
Reply