Where can I download the Android JB4.2.2 source?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I download the Android JB4.2.2 source?

2,006件の閲覧回数
zjuhasz
Contributor I

Hi,

Does anyone knows where the JB4.2.2 source is? The link 'IMX6_JB422_100_ANDROID_SOURCE' on page https://community.freescale.com/docs/DOC-94798 is not working.

Thanks.

ラベル(1)
0 件の賞賛
12 返答(返信)

1,168件の閲覧回数
Yuri
NXP Employee
NXP Employee

  I will send you the link.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

1,168件の閲覧回数
sheldonlrucker
Contributor IV

Hello Yuri,

Could you send me the link as well?  I need access to the JB4.2.2 source.  My email is sheldon_rucker@hotmail.com.

Thank you,

Sheldon

0 件の賞賛

1,168件の閲覧回数
Yuri
NXP Employee
NXP Employee

Done !

~Yuri.

0 件の賞賛

1,168件の閲覧回数
liuvincent
Contributor I

Hi Yuri,

I am working with iMX 6 EVB and need Android JB4.2.2 source also.

Can you please send my the link too?

Thank you,

Vincent

0 件の賞賛

1,168件の閲覧回数
Yuri
NXP Employee
NXP Employee

Your e-mail ?

~Yuri.

0 件の賞賛

1,168件の閲覧回数
charliechang
Contributor II

Could you send the android 4.2.2 source code download link to me? charliechang@aplex.com.tw

Thank you.

0 件の賞賛

1,168件の閲覧回数
Yuri
NXP Employee
NXP Employee

Done !

0 件の賞賛

1,168件の閲覧回数
liuvincent
Contributor I

Hi Yuri,

My email address is vincent.liu@u-blox.com

Thank you,

Vincent

0 件の賞賛

1,168件の閲覧回数
saurabh206
Senior Contributor III

Hi

Z

If you want JB4.3 than please follow

https://community.freescale.com/docs/DOC-99115

Thanks

Saurabh

0 件の賞賛

1,168件の閲覧回数
zjuhasz
Contributor I

Thanks Saurabh, but the problem is I need exactly the 4.2.2 version as other components I must use depend on this particular version. I might be able to move up t 4.3 or 4.4 later but first I must build m system using 4.2.2.

0 件の賞賛

1,168件の閲覧回数
saurabh206
Senior Contributor III

Hi,

You can download 4.3, once the download completed you can modified the manifest.xml for 4.2.2.

It should work.

Thanks

Saurabh

1,168件の閲覧回数
zjuhasz
Contributor I

Thanks, I will try that then.

0 件の賞賛