When will Android 4.4.3 BSP be released?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When will Android 4.4.3 BSP be released?

ソリューションへジャンプ
5,289件の閲覧回数
GregDyess
Contributor III

I have a need to run Android on a Linux 3.10 (or later) kernel for hardware support reasons.  I know the Android 4.4.3 in Freescale's repositories is using 3.10.? kernel.  I have the kernel and u-boot code from branch kk4.4.3_2.0.0-ga.  I'm still using the beta android patches from Freescale.  Unfortunately, it won't load Android. 

Does anyone know when (beyond just Feb-2015) the Android general availability release will be available?  This is becoming critical for us.

Thanks,

Greg

ラベル(3)
0 件の賞賛
返信
1 解決策
4,380件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Gregory,

It is scheduled for February 6th by end of day.

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
4,381件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Gregory,

It is scheduled for February 6th by end of day.

0 件の賞賛
返信
4,380件の閲覧回数
GregDyess
Contributor III

Where can I obtain the code and patches?

0 件の賞賛
返信
4,380件の閲覧回数
GregDyess
Contributor III

ooops, sorry.  I found it.

0 件の賞賛
返信
4,380件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

You can download it from here:

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Under: "Run time software" >> "operating system software" >> IMX6_KK443_200_ANDROID_SOURCE_BSP


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,380件の閲覧回数
simon_cai
Contributor III

Hi SergioSolis

I have downloaded the KK4.4.3 BSP.

but where I can fetch the documents for reference, something like IMX6_KK442_100_ANDROID_DOCS from i.MX 6 D/Q/DL/S/SL kk4.4.2_1.0.0 GA release

Thanks

Bateman

0 件の賞賛
返信
4,380件の閲覧回数
saurabh206
Senior Contributor III

Hi

Sergio

What will be the kernel version used?

0 件の賞賛
返信
4,380件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

I'm sorry for the late response, it is 3.10.53.


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信