When u-boot jump to serial downloader mode in u-boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When u-boot jump to serial downloader mode in u-boot?

Jump to solution
2,647 Views
kanoumamoru
Contributor III

Hello commuity,

 

I have one question concern with low level boot sequence.

 

Environment :

 - i.MX6DL @800MHz

 - DDR3 x 4pcs. (64bit bus)

 - SPI-NOR (u-boot and kernel)

 - eMMC (RootFS)

 

When SPI-NOR boot is selected:

  i.e. BOOT_MODE[1:0]=Internal Boot, BOOT_CFG1[7:4]=Serial ROM(SPI)

 

In this case, the system boot up sequence is as following :

  1. ROM code copy 4K byte data (include IVT and DCD table) from
      SPI-NOR to OCRAM.
  2. Init the DDR base on the DCD table settings.
  3. Copy and Load the u-boot form SPI-NOR to DDR.
  4. Jump to DDR to executes the u-boot.

 

A piece of DDR  was broken after ESD test, so DDR stress test became fail.

In other word, maybe above process 3, 4 (i.e.Copy and Load the u-boot / jump to DDR address) is not executed.

[Question]
In this case, the i.MX6 ROM BIOS will transition to the serial download mode?

 

Best Regards,

Kanou

Labels (3)
0 Kudos
Reply
1 Solution
2,368 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kanou

you are right: in this case i.MX6 ROM BIOS will transition to the serial download mode.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,368 Views
kanoumamoru
Contributor III

Hi Igor,

Thank you for replying.

My customer say:

If possible, Would you tell me how serial download mode is determined by the BIOS.

What kind of logic does it change in a serial downloading mode in?

For example, jump to exception interrupt handler, DDR CRC check error, ....

Best Regards,

kanou

0 Kudos
Reply
2,368 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kanou

yes ROM executes jump to exception interrupt handler.

Best regards
igor

0 Kudos
Reply
2,369 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kanou

you are right: in this case i.MX6 ROM BIOS will transition to the serial download mode.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply