When I run the same QT program and video (using mplayer)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When I run the same QT program and video (using mplayer)

2,341 Views
jongjupark
Contributor I

Dear community,

 

When I run the same QT program and video (using mplayer)
The video did not appear on the QT program, but the video covered the entire QT program.
Normal operation should be as shown in [normal operation] screen.

Why is this happening?

 

**description**

Kernel Version : L3.14.28

Application : QT

[Normal operation] : Samsung Exynos4412 Cpu, Kernel 3.8

movie_exynos.jpg

[Abnormal Operation] : NXP IMX6Q, Kernel 3.14.28

movie_nxp.jpg

0 Kudos
Reply
1 Reply

2,247 Views
igorpadykov
NXP Employee
NXP Employee

Hi jongju

one can try to follow sect.8.4 Qt 5 attached Linux Guide,

also please check useful link

I.MX-6 - Qt Wiki 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply