Hi!
What should I do to use fw_printenv/setenv on imx8mm?
【Conditions】
・hardware: imx8mm(on custom board)
・bsp: imx 6.1.55-2.2.0
・base image: core-image-minimal
・IMAGE_INSTALL += "u-boot-fw-utils"
・MACHINE = 'imx8mm-lpddr4-evk'
・boot storage:emmc
【log】
root@XXX:~# fw_printenv
Configuration file wrong or corrupted
root@XXX:~# strace fw_printenv
(omit)
openat(AT_FDCWD, "/etc/fw_env.config", O_RDONLY) = -1 ENOENT (No such file or directory)
write(2, "Configuration file wrong or corr"..., 38Configuration file wrong or corrupted
) = 38
exit_group(-9) = ?
+++ exited with 247 +++
root@XXX:~# fdisk -l
Disk /dev/mmcblk2: 7456 MB, 7818182656 bytes, 15269888 sectors
119296 cylinders, 4 heads, 32 sectors/track
Units: sectors of 1 * 512 = 512 bytes
Device Boot StartCHS EndCHS StartLBA EndLBA Sectors Size Id Type
/dev/mmcblk2p1 * 128,0,1 1023,3,32 16384 186775 170392 83.1M c Win95 FAT32 (LBA)
/dev/mmcblk2p2 1023,3,32 1023,3,32 196608 1596821 1400214 683M 83 Linux
/dev/mmcblk2p3 1023,3,32 1023,3,32 1605632 2968779 1363148 665M c Win95 FAT32 (LBA)
Disk /dev/mmcblk2boot0: 4 MB, 4194304 bytes, 8192 sectors
128 cylinders, 4 heads, 16 sectors/track
Units: sectors of 1 * 512 = 512 bytes
Disk /dev/mmcblk2boot0 doesn't contain a valid partition table
Disk /dev/mmcblk2boot1: 4 MB, 4194304 bytes, 8192 sectors
128 cylinders, 4 heads, 16 sectors/track
Units: sectors of 1 * 512 = 512 bytes
Disk /dev/mmcblk2boot1 doesn't contain a valid partition table
解決済! 解決策の投稿を見る。
This problem is solved.
1. The following is set in the config of u-boot.
CONFIG_SYS_MMC_ENV_DEV=2
CONFIG_SYS_MMC_ENV_PART=2
CONFIG_ENV_OFFSET=0x0
2. The following is set in /etc/fw_env.config
/dev/mmcblk2boot1 0x0 0x4000
N.B.
- CONFIG_SYS_MMC_ENV_DEV=2 means that there are u-boot-env in the mmcblk2.
- CONFIG_SYS_MMC_ENV_PART=2 means that there are u-boot-env in the mmcblk2boot1.
- CONFIG_ENV_OFFSET=0x0 means that u-boot-env is putted on no offset of the mmcblk2boot1.
- 0x4000 is default value of CONFIG_ENV_SIZE in imx8mm-evk.
- However, you cannot use fw_printenv/fw_setenv unless you run saveenv once in uboot or write u-boot-imx-initial-env-sd to mmcblk2boot1, because nothing is set in mmcblk2boot1.
This problem is solved.
1. The following is set in the config of u-boot.
CONFIG_SYS_MMC_ENV_DEV=2
CONFIG_SYS_MMC_ENV_PART=2
CONFIG_ENV_OFFSET=0x0
2. The following is set in /etc/fw_env.config
/dev/mmcblk2boot1 0x0 0x4000
N.B.
- CONFIG_SYS_MMC_ENV_DEV=2 means that there are u-boot-env in the mmcblk2.
- CONFIG_SYS_MMC_ENV_PART=2 means that there are u-boot-env in the mmcblk2boot1.
- CONFIG_ENV_OFFSET=0x0 means that u-boot-env is putted on no offset of the mmcblk2boot1.
- 0x4000 is default value of CONFIG_ENV_SIZE in imx8mm-evk.
- However, you cannot use fw_printenv/fw_setenv unless you run saveenv once in uboot or write u-boot-imx-initial-env-sd to mmcblk2boot1, because nothing is set in mmcblk2boot1.
You will face big problem saving env to eMMC boot partition than in user partition.
Hi, tavim.
Thanks for reply.
What kind of problem will be occurred?
You can refer to this Linux fw_printenv fw_setenv to access U-Boot's environment variables - NXP Community
I'm not sure where the address of uboot env is set...