What's the size of the cache line of i.MX6 quad Processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What's the size of the cache line of i.MX6 quad Processor

1,753 次查看
shijunzhao
Contributor III

What's the size of the L2 cache line of i.MX6 quad Processor?  I'm using an i.MX 6Quad SabreD board, and I have to know its size of L2 cache line.

I know most ARM CPUs use 64B cache line, but I see from some website that  the cache line is 32B on i.mx6q. Which is right? Thanks.

Below is the link of my board:

i.MX 6Quad SABRE Development Board | NXP 

Best Regards,

Zhao

标签 (1)
0 项奖励
回复
2 回复数

1,586 次查看
shijunzhao
Contributor III

Dear  igor,

Thanks for your reply. From the PL310 cache controller manual, I see that the cache line is 32B.

• Fixed line length of 32 bytes (eight words or 256 bits).

0 项奖励
回复

1,586 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Zhao

i.MX6Q L2 cache controller is described in sect.12.3.3 PL310 L2 Cache configuration

i.MX 6Dual/6Quad Applications Processor Reference Manual

and its characteristics can be found in PL310 Cache Controller Technical Reference Manual

https://static.docs.arm.com/ddi0246/b/DDI0246B_l2cc_pl310_r1p0_trm.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复