What maximum operating range of USB1_VBUS is support by i.MX8M Mini?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What maximum operating range of USB1_VBUS is support by i.MX8M Mini?

Jump to solution
1,229 Views
m_c
Senior Contributor I

In the page 18 i.MX8M Mini data sheet <http://nxp.com/doc/imx8mmiec>, it shows min/typ/max operating range of USB1_VBUS are 0.80/1.40/3.60v. In USB standard, VBUS is 5v. So what maximum operating range of USB1_VBUS is support by i.MX8M Mini?

Labels (1)
0 Kudos
Reply
1 Solution
1,129 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

datasheet is correct, usb connections are described in sect.3.9.14.1 Pad/Package/Board connections:


The USBx_VBUS pin cannot directly connect to the 5 V VBUS voltage on the USB2.0 link.
Each USBx_VBUS pin must be isolated by an external 30 K 1% precision resistor.

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,130 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

datasheet is correct, usb connections are described in sect.3.9.14.1 Pad/Package/Board connections:


The USBx_VBUS pin cannot directly connect to the 5 V VBUS voltage on the USB2.0 link.
Each USBx_VBUS pin must be isolated by an external 30 K 1% precision resistor.

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply