What maximum operating range of USB1_VBUS is support by i.MX8M Mini?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What maximum operating range of USB1_VBUS is support by i.MX8M Mini?

ソリューションへジャンプ
1,248件の閲覧回数
m_c
Senior Contributor I

In the page 18 i.MX8M Mini data sheet <http://nxp.com/doc/imx8mmiec>, it shows min/typ/max operating range of USB1_VBUS are 0.80/1.40/3.60v. In USB standard, VBUS is 5v. So what maximum operating range of USB1_VBUS is support by i.MX8M Mini?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,148件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

datasheet is correct, usb connections are described in sect.3.9.14.1 Pad/Package/Board connections:


The USBx_VBUS pin cannot directly connect to the 5 V VBUS voltage on the USB2.0 link.
Each USBx_VBUS pin must be isolated by an external 30 K 1% precision resistor.

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,149件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

datasheet is correct, usb connections are described in sect.3.9.14.1 Pad/Package/Board connections:


The USBx_VBUS pin cannot directly connect to the 5 V VBUS voltage on the USB2.0 link.
Each USBx_VBUS pin must be isolated by an external 30 K 1% precision resistor.

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信