What is the use case of "decoder_boot" and "encoder_boot" ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the use case of "decoder_boot" and "encoder_boot" ?

2,416件の閲覧回数
Raana
Contributor III

Dear Team,

 

I'm using 1GB DDR3 on our iMx8DX6 based custom board. Kernel version is, L4.14.62.

During analysis of current DDR/memory usage, we observed that Memtotal available is around 700 MB.

There the static allocation like shown in below line in dtsi file

               decoder_boot: decoder_boot@0x84000000 {

                        no-map;

                        reg = <0 0x84000000 0 0x2000000>;

                };

                encoder_boot: encoder_boot@0x86000000 {

                        no-map;

                        reg = <0 0x86000000 0 0x2000000>;

                };

etc...

 

mentioned in the structure of "reserved-memory" in "arch/arm64/boot/dts/freescale/fsl-imx8dx.dtsi" file.

 

We are not using Graphics & Framebuffer and still ~300MB is getting consumed by Kernel and with reserved/other components (i.e Memtotal is around 700MB – Checked using meminfo and free command).

We have modified the reserved size allocated for decoder_boot and encoder_boot and tested with this modified device tree file (dtb).

We could observe the increase in value of "MemTotal" (Memtotal confirmed using meminfo and free command).

 

Our observation is above fields are not affecting the board normal functionality.

Whether this "decoder_boot","encoder_boot","decoder_rpc","encoder_rpc" and "decoder_str" is really need to be reserved as we do not need to configure Graphics & Framebuffer ?

Please anybody can provide the exact use case of this field.

 

Best Regards,

J.P.Raja

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,331件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raja

these settings are for i.MX8DX VPU modules (encoder, decoder) described in sect.17.1.1.2 VPU

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

linux configuration in : linux/arch/arm64/boot/dts/freescale/fsl-imx8dx.dtsi

fsl-imx8dx.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

and sect.6.7.3 Menu Configuration Options attached Linux Manual.

It can be disabled if not used.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,331件の閲覧回数
Raana
Contributor III

Hi Igor,

I have already disabled all the configurations inside the "Device Drivers >MXC support drivers". But, No improvement.

So, now I have reduced the size of that. Like,

decoder_boot: decoder_boot@0x84000000 {
                        no-map;
                        reg = <0 0x84000000 0 0x4>;
};

encoder_boot: encoder_boot@0x86000000 {
                        no-map;
                        reg = <0 0x86000000 0 0x4>;
};

Reserved memory size also reduced now. Is this okay ?

Note: It was throwing error when I set as 0x0. That's why I set 0x4.

Thank You.

Best Regards,

J.P.Raja

0 件の賞賛
返信

2,331件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raja

one can try latest Linux L4.19.35_1.1.0
https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.19.35_1.1.0

Best regards
igor

0 件の賞賛
返信

2,331件の閲覧回数
Raana
Contributor III

Hi Igor,

Thanks for your reply. I'm unable to download the document (page not found).

Thank You.

Best Regards,

J.P.Raja

0 件の賞賛
返信