Hi Chu
Yes this is correct (as mentioned in RM and linux sources),
that the i.MX28 is able to drive LCD panel up to 800x480
resolution at 60Hz. Since both pixel pipeline and LCDIF do not impose any hard
maximum limit to 800x480, in general higher resolution LCD panel is allowed.
However, we do not recommend driving any panel with higher resolution than
800x480 due to limited internal bus bandwidth. In theory it is possible to run at a
higher resolution at lower frame rate (800x600 @ 48Hz is the same number of
pixels/sec as 800x480 @ 60Hz).
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------