What is the name and where is the i.MX6 VPU API located?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the name and where is the i.MX6 VPU API located?

2,670 Views
Sebster
Contributor II

Hello NXP,

 

Q1: Could you please let me know what is the name of the i.MX6 VPU API?

Q2: I’m told that it is only available in binary not in source. Could you confirm please?

Q:3 Where can I find it (and where is it located if it is in the imx6 Linux BSP)?

Q3: What is vpu_fw_imx6d.bin?

 

Thanks for your help.
Cheers

Seb

Labels (2)
0 Kudos
Reply
1 Reply

2,298 Views
igorpadykov
NXP Employee
NXP Employee

Hi Seb

please refer to attached VPU API document and

Linux Manual, Chapter 18 Video Processing Unit (VPU) Driver.

vpu_fw_imx6d.bin is firmware for VPU embedded BIT processor described in

Chapter 69 Video Processing Unit (VPU) i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply