What is the lowest power state for LPDDR SDRAM?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the lowest power state for LPDDR SDRAM?

ソリューションへジャンプ
1,795件の閲覧回数
nathanpalmer
Contributor IV

I have a legacy design that includes an iMX27 and LPDDR.  I am trying to take some measurements of the system power with various components powered off (or close to it) to calculate board overhead.  

I would like to disable the SDRAM, but I don't know if just not configuring it is enough to set it in the lowest power mode.  I am running application code from internal SRAM so I don't need the SDRAM at all.  How do I power it off (or close to off) from the iMX27?  Is there a mode I can put the SDRAM in that is essentially off?

Thanks!

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,522件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please use section 18.4.5 (Low Power Operating Modes) of the i.MX27 Reference Manual.
You can try Self Refresh Mode (section 18.4.5.1 Self Refresh Mode for SDRAM/LPDDR Devices)
or

Precharge Power Down Mode (section 18.4.5.3 Precharge Power Down Mode).

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,523件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please use section 18.4.5 (Low Power Operating Modes) of the i.MX27 Reference Manual.
You can try Self Refresh Mode (section 18.4.5.1 Self Refresh Mode for SDRAM/LPDDR Devices)
or

Precharge Power Down Mode (section 18.4.5.3 Precharge Power Down Mode).

0 件の賞賛
返信