It is not the error message, it just means Freescale MMCodec had been used, such information was generated by MMCodec in liscense checking.
Hi Qiang,
I modify the init.rc on my i.MX536 board, but the error is still appear.
# fsl omx graphic manager media framework property
setprop media.omxgm.enable-player 0
setprop media.omxgm.enable-record 0
setprop media.omxgm.enable-scan 0
Hi Pengru, You need check the runtime image to confirm the modification is there. In runtime Android system, use the followed command:
# cat /init.freescale.rc
Yes, I have get it on my runtime board:
#cat init.rc | busybox grep media
And I can see it.
where is init.rc? I not have..
Thank you.
It works ! the error messge disappears.
To disable the FSL codec, in init.rc, set the followed parameters to 0
# fsl omx graphic manager media framework property setprop media.omxgm.enable-player 0 setprop media.omxgm.enable-record 0 setprop media.omxgm.enable-scan 0
Could you tell me how to disable the mm-codec ?
I need to show it to customer to prove it's not system error.
Thanks.