What is the difference between the android AUTO version and the android Standard version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the difference between the android AUTO version and the android Standard version

ソリューションへジャンプ
2,008件の閲覧回数
dhty2015
Contributor II

What is the difference between the android AUTO version and the android Standard version?The same IMX8QM MEK board cannot be displayed on the ATUO version, while the standard version can be displayed normally.What is the difference between them, system differences or different requirements for hardware?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,907件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Yuelin,

They are complete different packages,. the code from Google for the Android Auto, has different Services that, Android Classic,  so even they have some similarities and use the same HAL, the configuration and setup, it is change because they are for different targets, and the i.MX8 family, has not been release yet, so the Android Classic it is the only BSP that has been fully tested.

Have a nice day sir!


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,908件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Yuelin,

They are complete different packages,. the code from Google for the Android Auto, has different Services that, Android Classic,  so even they have some similarities and use the same HAL, the configuration and setup, it is change because they are for different targets, and the i.MX8 family, has not been release yet, so the Android Classic it is the only BSP that has been fully tested.

Have a nice day sir!


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,907件の閲覧回数
dhty2015
Contributor II

What does EVS mean in the imx8 demo with or without EVS?Because when I use the auto version of android, the android without EVS can run normally, while the android with EVS does not display the output, but the serial port can enter the console.The board version is imx8qm mek, and the android version is android p9.0.0_1.0.2_auto_beta.Thank you very much!

0 件の賞賛
返信