I need to connect a cirtical hardware circuit whose control is from the processor. For the same i need to understand the status of the GPIO pin when the processor is in process of booting.
 
					
				
		
 art
		
			art
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Do you mean the i.MX6 series processors? If so, typically, their GPIO pins (except of some special purpose interface pins such as SDRAM interface pins) are by default configured as GPIO inputs with 100kOhm pull-up resistor enabled. You can exactly define the default pin state by reading the default values of corresponding IOMUXC register and corresponding GPIO controller register, that are listed in corresponding Reference Manual document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Arthur,
I need the information for iMX 283/287 processor.
Regards,
Shah Kunal
 
					
				
		
You can refer to the IMX6SLCEC-datasheet.pdf which download from the FSL website.
Hi Xlao,
I needed the information for iMX283/287 processors.
Regards,
Shah Kunal