What is the AES mode for HAB Encrypted boot?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is the AES mode for HAB Encrypted boot?

跳至解决方案
1,266 次查看
kanimozhi_t
Contributor V

Hi,

I would like to know the AES operation mode for the HAB encrypted boot?

From the "Security Reference Manual" we know the modes supported by AESA (AES accelerator in CAAM) and wonder what is the default mode used for the HAB Encrypted mode?

Can any one answer "What is the default AES mode for HAB encryption? and/or point us the the sensible reference?"

Thanks in advance.

0 项奖励
回复
1 解答
1,258 次查看
Yuri
NXP Employee
NXP Employee

@kanimozhi_t 
Hello,

  according to section 4.3.1.1. [Install Secret Key] of app note
"Encrypted Boot on i.MX6/7 series":

CAAM uses the AES-CCM algorithm for the encrypted boot.
[...] the key length specified in this section defines which variant to use.

https://www.nxp.com/webapp/Download?colCode=AN12056

 

Regards,
Yuri.

在原帖中查看解决方案

1 回复
1,259 次查看
Yuri
NXP Employee
NXP Employee

@kanimozhi_t 
Hello,

  according to section 4.3.1.1. [Install Secret Key] of app note
"Encrypted Boot on i.MX6/7 series":

CAAM uses the AES-CCM algorithm for the encrypted boot.
[...] the key length specified in this section defines which variant to use.

https://www.nxp.com/webapp/Download?colCode=AN12056

 

Regards,
Yuri.