What is max sustained USB 3.0 speed achieved?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is max sustained USB 3.0 speed achieved?

2,078 次查看
amuresan
Contributor III

When NXP created this chip, they characterized all peripherals.

What is the maximum sustained speed that the USB 3.0 actually achieved and which drivers were used?

0 项奖励
回复
3 回复数

1,746 次查看
joanxie
NXP TechSupport
NXP TechSupport

response from NXP Technical Support Services that said it was a USB / xHCI performance issue. The best we can do with USB 3.0 right now is 150-170 MB/s on all iMX6 & iMX8 platforms. They proposed to request their Professional Services in order to optimize USB 3.0 throughput.

0 项奖励
回复

1,746 次查看
amuresan
Contributor III

USB 3 is used by everyone.

You’re basically asking every single company to pay to unlock faster USB speeds. 

The ROCK64 chip can do 384MBytes/sec and it’s $35

0 项奖励
回复

1,746 次查看
amuresan
Contributor III

What exactly is the performance bottleneck?

the ROCK64 chip is $35 and it can do almost the full 3.2gbps that is practically achievable. 

So what is the bottleneck that NXP cannot overcome?

0 项奖励
回复