What is a input_reg in pinfunc.h and how it is derived ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is a input_reg in pinfunc.h and how it is derived ?

893 Views
santu_voonna
Contributor I

Hi All,

    I am pretty much new to IMX6SX and I have a basic query. Given a PAD and net name how to find out the input_reg which is mentioned in pinfunc.h ? 

#define MX6SX_PAD_NAND_CLE__ECSPI2_SCLK        0x014C    0x0494      0x0720        0x3         0x0

How could I derive from manual that input_reg is "0x0720" ??

Labels (1)
0 Kudos
Reply
1 Reply

799 Views
jimmychan
NXP TechSupport
NXP TechSupport

input_reg here is the register of Input Select for DAISY.

The offset address of IOMUXC_ECSPI2_IPP_CSPI_CLK_IN_SELECT_INPUT is 720h.

When DAISY set to 0, the clock input of ECSPI2_IPP_CSPI_CLK will be selected from the pad NAND_CLE (ALT3 mode).

For more details, please read the Select Input Register in the i.MX6SX Reference Manual.

0 Kudos
Reply