What does set i.MX6 HDMI display refresh rate?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What does set i.MX6 HDMI display refresh rate?

Jump to solution
1,292 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6 HDMI.

You know HDMI display refresh rate are several.

(e.g. 60.00, 59.94, 50.00, 23,98 Hz, etc...)

Then, what register determin the refresh rate?

HDMI module does not control and IPU DI controls it by VSYNC?

Best Regards,

Satoshi Shimoda

Tags (1)
0 Kudos
Reply
1 Solution
925 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes IPU controls it by VSYNC, providing data to HDMI,

one can look at example in IMX6DQRM Figure 33-4 and appnote below

shows how refresh is defined in LInux:

AN3974 Different Display Configurations on i.MX35 Linux PDK

sect.3.3.1.2 Panel Configuration, refresh rate

HDMI.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
926 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes IPU controls it by VSYNC, providing data to HDMI,

one can look at example in IMX6DQRM Figure 33-4 and appnote below

shows how refresh is defined in LInux:

AN3974 Different Display Configurations on i.MX35 Linux PDK

sect.3.3.1.2 Panel Configuration, refresh rate

HDMI.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply