What does seq_num mean in 802.1CB configuration?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What does seq_num mean in 802.1CB configuration?

793件の閲覧回数
liu8232303
Contributor I

in the document 《Real-time Edge Software User Guide.pdf》

bridge fdb add 7E:A8:8C:9B:41:DD dev swp0 vlan 1
tsntool> cbstreamidset --device swp0 --index 1 --nullstreamid --nulldmac 0x7EA88C9B41DD --
nullvid 1 --streamhandle 1
tsntool> cbgen --device swp3 --index 1 --iport_mask 0x08 --split_mask 0x07 --seq_len 16 --
seq_num 2048

4. Capture frames on swp2 on TestCenter.
We can get frames from swp2 on TestCenter, each frame adds the sequence number: 23450801, 23450802, 23450803…

【question】:

What does seq_num mean in 802.1CB configuration?seq_num 2048: is Initial value? 23450801 len is 4 bytes, exceed seqnum of R-TAG  2bytes?

 

0 件の賞賛
返信
1 返信

779件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

GEN_REC_SEQ_NUM: The sequence number to be used for outgoing packet passed to
SEQ_GEN function.
Note: Only lower 16-bits are sent in RED_TAG.

0 件の賞賛
返信